2025-07-16 4:06 PM
In my upcoming system I will be needing to use dynamic bitmaps.
Can dynamic bitmaps be located on the same RAM device (say SDRAM on STM32F469 discovery board) that is being used as the frame buffer?
I can carve out a piece of the SDRAM for the dynamic bitmaps, but is the DMA2D going to complain?
Thanks,
Andrei
Solved! Go to Solution.
2025-07-17 3:57 AM
Hello @Andrei Chichak,
If you have enough RAM it shouldn't cause an issue, but you might have some congestion because of a lot of read and write operations on the same bus. Using different memory banks for framebuffers and dynamics bitmap can help to reduce this issue.
BR,
2025-07-17 3:57 AM
Hello @Andrei Chichak,
If you have enough RAM it shouldn't cause an issue, but you might have some congestion because of a lot of read and write operations on the same bus. Using different memory banks for framebuffers and dynamics bitmap can help to reduce this issue.
BR,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.