2020-02-28 12:25 AM
I figured that ModalWindow can hijack touch buttons easily, but how can I do this for hardware buttons?
Is the only way to only call custom functions? So that in Designer I always use Interaction to call virtual function1, and route it like this:
function1(){
if (modalwindow1.isvisible())
{
... modal window handling
} else {
...normal application button handling, change Screen etc.
}
}This way I cannot use any of the default Interactions (change Screen etc.) in Designer, because they would act the same regardless of modal window is shown. So I have to route every screen change via virtual function call.
Would be nice if the modal window could override the handleKeyEvent()
Thanks!
Solved! Go to Solution.
2020-02-28 1:24 AM
There's nothing inherent in the functionality of the ModalWindow class that can do anything with hardware buttons.
There's a way to connect hardware buttons to interactions - would that do it for you?
/Martin
2020-02-28 1:24 AM
There's nothing inherent in the functionality of the ModalWindow class that can do anything with hardware buttons.
There's a way to connect hardware buttons to interactions - would that do it for you?
/Martin
2020-02-28 3:50 AM
>There's nothing inherent in the functionality of the ModalWindow class that can do anything with hardware buttons.
Ok. I think this would be as useful as hijacking touch events. Just like the ModalWindow does with touch events:
@class ModalWindow ModalWindow.hpp include/gui/common/ModalWindow.hpp
@brief Container for displaying a modal window and hijacking touch event to underlaying viewand widgets.(we don't have touchscreen in our product, only hardware buttons)
>There's a way to connect hardware buttons to interactions - would that do it for you?
Is this the system I proposed? E.g. map everything to virtual functions, which will check for the modal. Ok, I will use that. I should work, just needs a lot of repeated code, and I cannot use "change screen" in designer (because it will change screen regardless of modal window).
2020-02-28 4:16 AM
What "hijacking touch events" means is simply that it's an overlay, and as such, things that are below it won't receive touch events. The description is a bit convoluted.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.