STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Can ModalWindow hijack hardware button handling?

I figured that ModalWindow can hijack touch buttons easily, but how can I do this for hardware buttons?Is the only way to only call custom functions? So that in Designer I always use Interaction to call virtual function1, and route it like this:funct...

Tuoman by Senior II
  • 1893 Views
  • 3 replies
  • 0 kudos

Resolved! IBUSERR with emWIN on STM32F4?

I need some advice on how to solve an issue with a forced hard fault IBUSERR when using ST provided emWIN freeware on a custom designed STM32F429BI based board. The STM32F429 is running HSI at 168MHz at 3.3v. As shown below, the forced hard fault I...

0690X00000DXNYdQAP.jpg

STM32F746GDISCOVERY and TouchGFX 4.13 problem

Hi to all i have this problem, i create a simpe example with TouchGFX Designer 4.13, i use the STM32F746GDISCOVERY for my test.I create the esample and i see all work well because i run simulator and run target all work well.I generate the code, i op...

antonioB by Associate II
  • 1359 Views
  • 2 replies
  • 0 kudos

Resolved! How to choose QSPI Flash(nor flash or nand flash)and ram on stm32h7b0vb is enough for custom design?

Hi,I have a project under EVT situation.I will choose the stm32h7b0vb(128K Flash + 1.18M SRAM)as the mcu for the system.The main functions is below:1,Driver a tft-lcd with touch via LTDC interface,lcd size is 640*360 pixes support rgb888 and support ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.