2021-10-07 10:03 AM
Hello,
I'm working with touchGFX and I'm a beginner in it.
Please do not mind if the question is not proper.
I have generated a code using touchGFX but the code generated is in cpp language.
Is there any way if I can code for touchGFX in c language.
Thank you in advance.
Solved! Go to Solution.
2021-10-07 10:40 AM
When you ask control GUI parts in C, then simple reply is it cant.
When you ask for RTOS other tasks except GUI, you can use C in some tasks C++ in other usw...
2021-10-07 10:32 AM
Generally it's going to be easier to adopt the language of the auto generated code. Certainly most C code can run perfectly well within a CPP file.
2021-10-07 10:40 AM
When you ask control GUI parts in C, then simple reply is it cant.
When you ask for RTOS other tasks except GUI, you can use C in some tasks C++ in other usw...
2021-10-08 5:07 AM
Thank you for the quick response.
I'm trying to debug the code for TouchGFX from stm32cubeide (1.7.0) to the stm32h757i-eval board.
The debug happens successfully but there is nothing being displayed on the board.
this is the response after debug
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-Link Server is running on port : 7184
ST-LINK SN : 003600263137510F33333639
ST-LINK FW : V3J8M3
Board : STM32H757I-EVAL
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a01420.srec
File : ST-LINK_GDB_server_a01420.srec
Size : 468880 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 3]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:05.389
Verifying ...
Download verified successfully
The debug is successful but
the code is not running on the display.
Thanks in advance.
2021-10-09 3:43 AM
"The debug is successful but
the code is not running on the display."
Maybe you mean flash is successful, because debug is real check , that code is run and loop in normal.
Download verified dont mean that code is realy started usw.
What code you load to H757 ? Custom or original example?
Good point to start is ready to go example in TouchGFX if exist for your board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.