STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Show multiple lines in touchGFX text area

Hi,I would like to show dynamic text in text area with wildcard. The text contains the 'new line' character (\n) to jump to next line. for example: "First Line \n Second Line " will be printed to screen:First LineSecond LineTouchGFX does not recogniz...

ari_v2 by Senior
  • 2406 Views
  • 2 replies
  • 0 kudos

Resolved! can I code in c language for touch GFX?

Hello,I'm working with touchGFX and I'm a beginner in it.Please do not mind if the question is not proper.I have generated a code using touchGFX but the code generated is in cpp language.Is there any way if I can code for touchGFX in c language.Thank...

Aarra.1 by Senior
  • 2967 Views
  • 4 replies
  • 0 kudos

Include problems with TouchGFX

Hello everyone,I'm working on a new project using TouchGFX in STM32CubeIDE, I don't understand why I have include problems, especially that a file is recognized in one file and not in an other...Here is my includes : I've got these errors :What is we...

0693W00000FBsBtQAL.png 0693W00000FBs4oQAD.png 0693W00000FBsDQQA1.png 0693W00000FBsDfQAL.png
MLair.1 by Associate III
  • 1487 Views
  • 1 replies
  • 0 kudos

Undefined reference to image (TouchGFX)

Hi,I'm trying to add an image. Touchgfx is generating the code fine but when I compile the stm32cubeide it says "undefined reference to `image_icon_hourglass' ". Can anyone share their thought on what it could be?

Ofaro.1 by Associate II
  • 1262 Views
  • 3 replies
  • 0 kudos

Resolved! TEXT PROGRESS Negative Values

Hi,I'm trying to display the temperature values ranging from -40 to +40 on TEXT PROGRESS in TouchGFX designer. Unfortunately, the values range only starts from 0.Can anyone help me with this? I'll be very grateful.

Ofaro.1 by Associate II
  • 3458 Views
  • 7 replies
  • 0 kudos

Resolved! TouchGFX with dual core support.

I would like to know when touchgfx team can launch touchgfx with dual core support. I have 747I-disco and am using CubeIDE, but this is the question asked a month ago. I got an answer from touchGFX team we could get the support by the end of Jan, but...

JKing.2 by Associate II
  • 2925 Views
  • 4 replies
  • 0 kudos

Resolved! ToouchGFX Getting button ID

Hi,I want to set a common interaction for all buttons on screen. For this, I configured button interactions to call the same virtual function ButtonClicked(). How could I determine in this function, which button was clicked? Is there a way to tell To...

ari_v2 by Senior
  • 3259 Views
  • 2 replies
  • 0 kudos

"No such file or directory" error: STM32F429I-DISC1

Greetings AllI am implementing an ADC-based GUI on my board and my code is not building due to the abovementioned error (even when the file exists. I am using STMCubeMX(6.3.0), STM32CubeIDE (1.7.0) and TouchGFX(4.17.0) to develop my GUI. Most of thes...

LNdungane by Associate II
  • 7192 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.