2024-09-26 8:44 PM
Hi, I went through some other discussions discussing a similar problem, but they did not seem to help.
I have screen one which displays (dynamically) a container. The container has a button on it, which when clicked, changes screens to screen 2. At the same time the container needs to send data to screen 2 (an int). The button is a flex button which I set up from the GUI call a virtual function.
I would prefer a way where the container is not permanently tied to screen 2, as this container appears on multiple screens and does something similar.
Solved! Go to Solution.
2024-10-04 2:07 AM - edited 2024-10-04 2:07 AM
Hello @Priyank ,
Did you solve this issue?
I saw that you created a new topic (the new topic ).
If you did, I invite you to select the comment that was the most helpful (if any) as "best answer". :smiling_face_with_smiling_eyes:
Regards,
2024-11-19 2:15 PM - edited 2025-03-11 2:18 PM
While studying this how to pass information from Widget/View/Presenter/Model.
I've been struggling with the callbacks.One of the thing I found was the use of Canvas to allocate memory beforehand for dynamic widget creations.Check Demo2/HomeAutomationView()/CanvasWidgetRenderer as an example.(This one is going to he complicated, check the MVPHeader for possible "global" memory.)Did you figure out a way to have interactions between a customWidget/View back and forth without having to make many callbacks?
Edit: I couldn't find a way to have a global memory arena (can't use mallocs/free) that I could spawn widgets into dynamically. I conceded to use a small number of items and always allocate that number of widget into a page.
I add and remove them from the View/Screen dynamically.
2024-11-21 6:44 AM
Hi, I did find the solution, it still uses callbacks, however they are generated callbacks. I used this tutorial right here, where you would utilize actions, triggers, and interactions.
https://support.touchgfx.com/4.18/docs/tutorials/tutorial-05
2024-11-21 8:40 AM
Thanks for the reference but I found a solution yesterday.
For posterity:
The gist of what I understood it is:
Context switching ties in with the MVP.
I used "Demo2" and "Understanding Application Structure" to finally get it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.