2020-11-19 6:56 AM
Hello,
I cannot use correctly TouchGFX Designer. When I use "run Target", when arriving at the step of stmCubeProgrammer, I have this issue :
...
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0
-------------------------------------------------------------------
Error: External loader c:\program cannot be loaded.
Error: External loader files\stmicroelectronics\stm32cube\stm32cubeprogrammer\bin\externalloader\n25q128a_stm32469i-disco.stldr cannot be loaded.
ST-LINK SN : 066EFF3530384E5043221930
ST-LINK FW : V2J36M26
Board : 32F469IDISCOVERY
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x434
Revision ID : Rev A
Device name : STM32F469xx/F467xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
....As you can see the path for the external loader path is splited in 2 parts because of the space in "Program Files". It seems that I am the only one with this issue ? I did not have this issue with the previous release of TouchGFX.
Solved! Go to Solution.
2020-12-17 4:01 AM
Hi @Svenn Dahlstrom ,
CubeProgrammer team is fixing this, but in the meantime you can either use 2.5 and be happy, or.... i'm publishing a known issue for cubeprogrammer 2.6 to make it work with TouchGFX makefiles (which works since its from command-line as you mention).
/Martin
2020-11-19 7:30 AM
Hi, i'll investigate if this is an issue with CubeProgrammer 2.6.0. That seems to be an internal error message.
/Martin
2020-11-19 7:37 AM
<sarcasme> Spaces and backslashes in filennames are such a great achievment</sarcasme>
2020-11-19 7:41 AM
@Martin KJELDSEN , I updated CubeProgrammer because I thought it was the issue. Thus, I had the same problem with previous release of CubeProgrammer.
I also reinstalled TouchGFX to the default folder just in case ^^
2020-11-20 2:24 AM
Oh, okay! That's really strange. There must be an internal refernce in cubeprogrammer to the loader files (stldr) but it fails because its inside program files. That's never been a problem here. I have 32-bit and 64-bit versions installed in both program files and program files (x86)
2020-11-20 2:27 AM
I added this post to the STM32CubeProgrammer community as well
2020-11-20 3:11 AM
Do you mean that I am the "only" one having this issue ?
Can I test something to resolve this issue then ? Reinstall something with a previous release, or something else ?
Thank you.
2020-11-20 4:11 AM
It's not something I've heard about before, no, hmm. I'm not an expert on CubeProgrammer to be honest.
I've added the CubeProgrammer topic to the post. Let's see if we can get some answers.
/Martin
2020-11-20 5:43 AM
For the people more aware of STM32CubeProgrammer side. When using with the GUI (ie not with TouchGFX), I have no problem to add the external loader (by checking the right light under the "External loaders" menu) when connecting to the board. And thus, I can flash successfully the binary created by TouchGFX and I have the correct interface I have designed.
2020-11-24 12:19 AM
Hello @Martin KJELDSEN ,
I used the STM32CubeProgrammer CLI to test if it is TouchGFX related. And it is not. I have the same problem. Strangly, as I said, I don't seem to have the problem when using the CubeProgrammer GUI.
Should I create a new topic because it has nothing to do with TouchGFX ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.