2019-02-26 7:16 AM
I created a custom container in which I placed a scrollwheel.
I added in the item template and selected item template both of which use text with wildcard placements.
The problem arises when I select these text widgets to use a wildcard buffer at which point multiple identically named buffers are defined in the controls base class which cause the compiler to fail.
I have replicated in a small project whch I can zip and email if you say who can deal with this.
Solved! Go to Solution.
2019-03-07 1:10 AM
Hi @brianshankland9,
This issue was present in 4.10.0 but has been fixed in 4.11.0.
2019-03-06 4:43 AM
Hi @brianshankland9,
Please share the project with me. How do you want to do it? Which version of TouchGFX is this?
(Thanks for your report. I'll gladly check to see if you're right)
Best regards,
Martin
2019-03-07 1:10 AM
Hi @brianshankland9,
This issue was present in 4.10.0 but has been fixed in 4.11.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.