2020-12-11 12:37 PM
I've created a project using STM32H7B3I-DK eval board with all settings default, unmodified, taken from TouchGFX. UI menu is working fine with some resources stored in OSPI Flash memory.
Now I wish to store some data in this OSPI memory. The procedure should be to disable Memory Mapped Mode, erase, write and enable Memory Mapped Mode again. All this I do with task switch disabled so that TouchGFX doesn't access OSPI Flash during the process. But BSP_OSPI_NOR_Erase_Block() returns error.
Ccalled are MX25LM51245G_BlockErase()
then HAL_OSPI_Command()
then status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_TC, SET, tickstart, Timeout);
and here timeout is reported.
I've tried to erase OSPI Flash even before TouchGFX is started and it fails too.
Here is my simple code called from main with just one modification:
static void MX_OCTOSPI1_Init(void)
{
/* USER CODE BEGIN OCTOSPI1_Init 0 */
/* USER CODE END OCTOSPI1_Init 0 */
/* USER CODE BEGIN OCTOSPI1_Init 1 */
/* USER CODE END OCTOSPI1_Init 1 */
/* OCTOSPI1 parameter configuration*/
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThreshold = 1;
hospi1.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
hospi1.Init.MemoryType = HAL_OSPI_MEMTYPE_MICRON;
hospi1.Init.DeviceSize = 26;
hospi1.Init.ChipSelectHighTime = 2;
hospi1.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 3;
hospi1.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_DISABLE;
hospi1.Init.ChipSelectBoundary = 0;
hospi1.Init.ClkChipSelectHighTime = 0;
hospi1.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_BYPASSED;
hospi1.Init.MaxTran = 0;
hospi1.Init.Refresh = 0;
if (HAL_OSPI_Init(&hospi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN OCTOSPI1_Init 2 */
BSP_OSPI_NOR_Init_t Flash;
Flash.InterfaceMode = BSP_OSPI_NOR_OPI_MODE;
Flash.TransferRate = BSP_OSPI_NOR_DTR_TRANSFER;
BSP_OSPI_NOR_DeInit(0);
int32_t RetVal = BSP_OSPI_NOR_Init(0, &Flash);
if(RetVal != BSP_ERROR_NONE)
{
Error_Handler();
}
/**************************************************************/
BSP_OSPI_NOR_Erase_Block(0, 0x90000200, MX25LM51245G_ERASE_4K); //that's the only modification, it fails with timeout, then enabling memory mapped mode below fails too
/**************************************************************/
RetVal = BSP_OSPI_NOR_EnableMemoryMappedMode(0);
if(RetVal != BSP_ERROR_NONE)
{
Error_Handler();
}
/* USER CODE END OCTOSPI1_Init 2 */
}
Solved! Go to Solution.
2020-12-14 12:14 PM
Answering to myself:
everything is working fine, the simple mistake was in my address calculation. BSP_OSPI_NOR_...() functions must get Flash Memory address starting from 0 and not with +0x90000000 offset, as CPU sees it.
So I can confirm, that switching from Memory Mapped Mode, erasing, writing and enabling MMM again is fully functional.
2020-12-14 12:14 PM
Answering to myself:
everything is working fine, the simple mistake was in my address calculation. BSP_OSPI_NOR_...() functions must get Flash Memory address starting from 0 and not with +0x90000000 offset, as CPU sees it.
So I can confirm, that switching from Memory Mapped Mode, erasing, writing and enabling MMM again is fully functional.
2022-10-30 5:14 PM
Hi @Tomasz Ozon I just wanted to say thanks for posting your answer as this was exactly my problem and your post saved me untold hours in solving this!
2022-10-30 8:17 PM
Yes
sCommand.Address = Address & 0x0FFFFFFF; // 256 MB masking
One should also watch this on the External Loaders, and probably ensure all checks and comparisons are done with masked addresses. Things passed in are not always zero based, the Erase range has caused me headaches in the past. Might have been fixed along the way.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.