STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! BSP_OSPI_NOR_Erase_Block() fails

I've created a project using STM32H7B3I-DK eval board with all settings default, unmodified, taken from TouchGFX. UI menu is working fine with some resources stored in OSPI Flash memory.Now I wish to store some data in this OSPI memory. The procedure...

Resolved! Issue with latest X-CUBE-DISPLAY

I'm using a NUCLEO-L476RG with a X-NUCLEO-GFX01M1 (MB1642-DT022CTFT-B01). With X-CUBE-DISPLAY v2.0.1, it works fine, but with v2.2.0, after reset, the display just flickers. Any ideas?

paswenson by Associate II
  • 3216 Views
  • 6 replies
  • 0 kudos

STM32F746 touchgfx and USB don't work

I am not able to use both USB (CDC or MSC class tested) and touchgfx (GUI) in my device which consist of: STM32F746, 800x600 touchscreen, external qspi flash for assets, external sdram and other peripherals like spi or i2c. Firmware is based on freer...

BMich.2 by Associate
  • 3501 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX 4.20.0 working with CubeIDE 1.10.1, how do I open and work with the TouchGFX project in CubeIDE?

I'm using a STM32F429I-DISC1 board. I can create a display in TouchGFX and it creates the project in the default location "C:\TouchGFXProjects\Display". It makes an IOC file in the "Display" folder "STM32F429I_DISCO_REV_E01.IOC" It makes a "STM32C...

SWood.4 by Associate III
  • 2356 Views
  • 3 replies
  • 0 kudos

Stm32F427 with external SDRM and external NOR flash. 2mB of SDRAM is used as frame buffer for LCD. this is a working system. In some faulty bords, the system misbehaves.

In particular, I can see random white dots on LCD when external NOR flash is written, like writing in the flash somehow influence the frame buffer. Testing RAM for error passes OK, same is when I test NOR flash write and verify. I searched for a prob...

Johanan1 by Associate II
  • 4379 Views
  • 8 replies
  • 0 kudos

I have a problem in my TFT LCD project. I use LTDC, FMC, SDIO, and Touchgfx. I read all of the images in stm32f429 from the SD card. some of the images in my project don't load correctly. what should I do? and what is the reason?

as shown in this picture (the top picture is in Touchgfx and the bottom picture is in my LCD board) some images in my LCD don't load correctly!my code :void StartDefaultTask(void const * argument)   {   /* USER CODE BEGIN 5 */     f_mount(&SDFa...

0693W00000Subh1QAB.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.