2022-04-05 3:04 AM
<STM32CubeF7-master\Projects\STM32F7508-DISCO\Examples\BSP>
<STM32CubeF7-master\Projects\STM32F7508-DISCO\Examples\LTDC>
after few seconds code stops with error (refer attached img file)
2022-04-05 5:39 AM
Hello @Ss.6 ,
Make sure that you have program the internal Flash with the ExtMem_Boot (Path: Projects\STM32F7508-DISCO\Templates\ExtMem_Boot).
In order to make the example work, you must do the following:
1. Select required configuration in memory.h in Templates\ExtMem_Boot\Inc.
The default configuration is the right one:
- DATA_AREA set to USE_INTERNAL_SRAM
- CODE_AREA set to USE_QSPI
2. Program the internal Flash with the ExtMem_Boot.
3. Program the external memory with this example "Examples/BSP".
4. Start debugging user example or reset for free running.
Otherwise, you can find all the steps to run the example in the README file.
I hope this helps.
BeST Regards,
Walid
2022-04-05 6:41 AM
There really needs to be some robust QA to ensure that examples all work out of the box.
2022-04-05 8:31 PM
Thank you very much for quick response,
yes ,
<it shows the error attached image>
regards
sivanesh
2022-04-05 8:34 PM
The query,
How to debug the code in external memory?
Is the same procedure open the project and do the debug or any other methods?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.