2019-12-18 3:41 AM
Hi,
I am using TouchGFX 4.10 with STM32F769 on a custom board. My graphics includes 2 archs and 2 gauges (added as png) that must be rotate and two counters in the format HH:MM
When the system is active, counters must have “:�? blinking @2Hz and gauges and archs must move.
To move gauges I am using gaugeX.updateAngles(0.0F, 0.0F, zAngle2D_x); and to move archs i am using arcX.updateArcEnd(ARCH_END_x);
All is in the main routine void monitorView::handleTickEvent()
No issue in moving gauges and archs… the problem is that blinking is stopped when archs and/or gauges are moving.
It seems that updateAngles and updateArcEnd are blocking till these routine are ended.
Any suggestion on how to solve this are welcome.
Thanks
2019-12-19 1:02 AM
Hi,
Something else is wrong. Nothing should be blocking - It works a bit different than what you think, i think. I think i'll need to see some screenshots, some code, etc.
/Martin
2019-12-19 1:11 AM
Hi Martin,
thanks for your answer.
I agree with you that there is something wrong in my code (it is my first TouchGFX project) and not with TouchGFX
Due to company rule, I can not share here all my code.. can I send you it in a private email? Of course when I solve the problem, I will share the solution
Thanks
Dario
2019-12-19 1:16 AM
I understand. How about sending it in a private message here? I'll take a look at it when i can but i'm a biiit tied up at the moment.
2019-12-19 1:26 AM
Hi Martin,
ok. I will prepare the files and I will write you
Many thanks
Dario
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.