STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32F7 DCMI support for output mode?

Posted on July 02, 2015 at 12:21Reading the reference manual RM0385 (DocID026670 Rev 1) in the introduction to the DCMI on p. 478 I encountered this: ''[...] This interface is also able to transmit a parallel data flow, allowing it to emulate a came...

arne by Associate II
  • 2756 Views
  • 6 replies
  • 0 kudos

How to integrate touchgfx with keil ?

hi I make a very basic project in touchGfx works fine in stm32f746 disco board when load from TouchGfX directly . After that i run stm32Cube project located on my touchgfx folder and generate code foe keil . When i start to build the code i got some ...

SIsla by Associate
  • 1928 Views
  • 2 replies
  • 0 kudos

TouchGFX migration from STM32F7 to STM32H7

We are using STM32F7 with TouchGFX and considering in migrating it to STM32H7 series. May we know how much effort is needed to migrate those TouchGFX things from STM32F7 to STM32H7? Is it easy?Thanks.

S.P. by Associate II
  • 1268 Views
  • 2 replies
  • 0 kudos

TouchGFX Error on SW4STM32

Hi, i'm working on my first project that i use touchGFX, i used ST tutorial to generate code for Eval Board STM32F429I-EVAL. i have an execution error : ../TouchGFX/simulator/main.cpp:30:22: fatal error: shellapi.h: No such file or directory This er...

elguezzar by Associate II
  • 2817 Views
  • 7 replies
  • 3 kudos

BMP to RGB565

Hi. I’m trying the DMA2D example on the STM32L496G-DISCO board.Can anyone tell me where to find the software tool to convert a picture to the RGB565 Array that is used in this example?Hope you can help thanks in advance.

spa23 by Associate III
  • 1238 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.