STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

moving to different package STM32F429ZI -> STM32F429II, is there anything to change on TouchGFX BSP?

hi, i'm developing a TouchGFX Designer based app on STM32F429I-DISC1 that's based on STM32F429ZI LQFP144 pin MCU. so far so good, but..we need more IO pins to they told me our custom board will be based on STM32F429II which is LQFP176. i asked them t...

Resolved! Keil folder doesnt exist

Hi guys, I have a STM32L4R9I-DISCO board. I create a touchgfx project from Application Template for this disco board. After that I can run simulator, generate code and run target without problem. I can see my application in disco board's LCD. I wi...

Epamuk by Associate III
  • 1557 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 5.1.0 generate incorrect code for LCD

Hi,there is a bug of CubeMX I Found:I’m using STM32CubeMX5.1.0,and STM32CUBE_FW_L0_V1.11.0when creating a project for stm32l073, In ‘LCD Mode and Configuration’ dialog, ‘Multiplex Mode’ checkbox takes no effect. Whether it is checked or not, CubeMX ...

CGuo by Associate
  • 1514 Views
  • 1 replies
  • 0 kudos

Adafruit Color TFT with Nucleo H743

Has anyone got the Adafruit 1.8" Color TFT Shield to work with a Nucleo H743?I have tried the demonstration program from the STM32Cube_FW_H7_V1.3.0 package that supports this board, but nothing is displayed. I have verified that SPI data is being sen...

Chris1 by Senior III
  • 2446 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.