STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Error when using custom widget.

Hey.I'm trying to use a custom widget. Error:---------------------------Microsoft Visual C++ Runtime Library---------------------------Assertion failed!Program: ...mulator\msvs\..\..\build\Debug\bin\Application.exeFile: ..\..\..\..\framework\source\t...

Hosting by Associate III
  • 1207 Views
  • 1 replies
  • 0 kudos

Reducing Bus Arbitration SlowDown on Simultaneous DCMI (via DMA), LTDC (via APB2), and SDMMC (via APB2) Utilization of FMC Data

All,I have been utilizing the STM32F765 chip to transfer frames (RAW images) of data back and forth from a camera, to flexible memory RAM, to the screen, to/from an SD card. When I attempt to use the DMA in tandem with interrupt based transfers to an...

ZThat by Senior
  • 844 Views
  • 0 replies
  • 0 kudos

how to reset the settings of stm32cubeMX

Hello, in "graphics / touchGFX", I made a mistake, I selected my project touchGFX instead of selecting the .exe software. Now I can not select the right because the "type of files" is blocked on the name of my project ... I tried to reinstall Stm32Cu...

RBECA by Associate
  • 1790 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.