STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

32F429IDISCOVERY-DISCO1 problem with compilation

HiI am trying to use TouchGFX with my 32F429IDISCOVERY, DISCO1 according to the video https://www.youtube.com/watch?v=VOs2LYO7wSA) and the description https://touchgfx.zendesk.com/hc/en-us/articles/360021620431-Configuring-STM32F429I-DISCOI use STM32...

Artur_B by Associate II
  • 4387 Views
  • 10 replies
  • 0 kudos

touch gfx TEXT type

Hi,There is an example in touch gfx designer named "TouchGFX Demo 2". There is carousel for swiping the icons, while swiping icons, there is a text swiped below icons in MainMenuCarousel page. This text is constant and is defined as TEXT type, so we ...

er3481 by Senior
  • 915 Views
  • 1 replies
  • 0 kudos

I created a custom keyboard (as seen as in the TouchGFX examples), but even before I enter the last Screen, where it should be visible, it appears on the screen before. But why?

Screen3View.hpp (Where the keyboard should be visible) #ifndef SCREEN3VIEW_HPP   #define SCREEN3VIEW_HPP     #include <gui_generated/screen3_screen/Screen3ViewBase.hpp>   #include <gui/screen3_screen/Screen3Presenter.hpp>   #include <gui_generated/sc...

MWetter by Associate III
  • 905 Views
  • 1 replies
  • 0 kudos

Resolved! Canvas Widget Renderer error

I tried to implement a view (box+grid+graph) in vs. The grid consists of many lines and the graph is inherited by CanvasWidget.1. Create canvasBuffer[CANVAS_BUFFER_SIZE] in main. cpp;Graph alone is ok.CanvasWidgetRenderer: : setupBuffer (canvasBuffer...

lxw by Senior
  • 1521 Views
  • 2 replies
  • 0 kudos

Hardware STM32F746 using TouchGFX for TFT 7 inch

Hi everyone.I'm beginning with STM32F746 Discovery Kit, I already build some app using TouchGFX run on this Kit.Now I want to build a new hardware for my app based on STM32F746 kit, but I will using TFT 7 inch (800x400).Because I will solder my pcb​,...

HAnh by Associate III
  • 2886 Views
  • 6 replies
  • 0 kudos

DCMI only triggering line interrupt

I have an OV7670 camera that I am trying to capture images with. I am able to communicate with and set registers for the camera. When power, GND, and XLCK (16 MHz) pins are supplied to the pin I am also able to detect that proper image data is bein...

Cause of Overrun Error (OVR) in DCMI

So I want to briefly explain my project. I am using STM32F746 MCU for my smart home project. In this project I have to include live stream from a PAL camera. I am using a TW9912 to get 8 bit progressive YCbCr after which I convert to RGB and display...

SLavi by Associate II
  • 2986 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.