2020-01-13 5:25 AM
I wanted to use the example "Method 1 - From GUI task" TouchGFX. I downloaded PollDemoHwInt 4.9.3.zip. Unpacked. Can't open STM32CubeIDE 1.1.0?
2020-01-15 12:37 AM
The example is based on 4.9.3 and was written before CubeIDE came out, i think. I'm guessing the reason you can't open it is because there's no cube ide project.
Please enlighten me if i'm wrong.
/Martin
2020-01-15 2:36 AM
This is. Can this be remedied?
2020-01-15 2:42 AM
Unfortunately not. At least not by us, right now. Which board are you going to try this on? And what are you trying to accomplish? I may be able to guide you in the right direction - E.g. the new v3 Application templates already come with .ioc files that you can open and configure additionally through CubeMX and generate a CubeIDE project. Then make your modifications for hardware integration with touchgfx according to the example you've just downloaded for inspiration,
/Martin
2020-01-15 9:24 AM
I came back to STM32CubeIDE 1.1.0. I am happy with that, therefore I will not return to version 1.2.0. I work on STM32F746G-DISCO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.