STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Generated Font Naming

Hi,Follwing Font cpp files are being generated:Font_Ubunut_light_10_4bpp_0.cppFont_Ubunut_light_10_4bpp_4.cppFont_Ubunut_light_16_4bpp_0.cppFont_Ubunut_light_16_4bpp_4.cppMy question: What does the _4 (in bold) mean? Why are there different font wit...

jimmii by Senior II
  • 1800 Views
  • 3 replies
  • 0 kudos

concept of layers

Hello.Does TouchGFX have the concept of layers?For example, is it possible to put the keyboard window on the upper layer of the main screen when in key input mode?Thank you.

Ebun.1 by Senior
  • 1995 Views
  • 4 replies
  • 0 kudos

STM32F746G and touchGFX problem whit IAR and CubeIDE

Hi to all, i want to try a TouchGFX i create a simple example, i use CubeMX and select X-Cube-TouchGFX 4.13.0 for additional software, i configure all well, i see example and webinar for configure it and use TouchGFX designer for insert a simple UI f...

antonioB by Associate II
  • 1988 Views
  • 4 replies
  • 0 kudos

STM32F4 Discovery - DCMI does not call HAL_DCMI_FrameEventCallback Camera : ov9655 I am using CubeMX to generate the code

Hello There,I am trying to connect OV9655 camera (WaveShare) module with STm32f4 discovery board. After generating files from CubeMX and importing ov9655 drivers (ov9655.h & ov9655.c) I am able to get HAL_DCMI_LineEventCallback and HAL_DCMI_VsyncEven...

Junaid by Associate II
  • 9829 Views
  • 16 replies
  • 0 kudos

SCREEN PROGRAMMING WITH MCU PROGRAMMING

Hello I'm still newbie in stm and i'm using a STM32F429zi discovery board.I've did programming a little about gpio, adc, spi, pwm, usart, i2c.As you can see i've done with basic interface .So now I want use graphic touch LCD which is attched on the b...

SKim.1761 by Associate III
  • 723 Views
  • 0 replies
  • 0 kudos

STM32H750VBT6 can't work LTDC function

I was use CubeMX create a LTDC function for STM32H750VBT6my steps:1.Open CubeMX2.MCU Select:STM32H750VBT63.Function Select:RCC�?LTDC�?DEBUG�?SPI6�?FREERTOS4.Generate Code to create a new project5.Open this project by IDE6.Download and Run7.CrashI exe...

0690X00000D9vstQAB.jpg
eric.hsu by Associate II
  • 2137 Views
  • 2 replies
  • 0 kudos

Resolved! Problem using QSPI with STM32F746 and TouchGFX

Hello!I repost my question here as I posted it in an answer yesterday and it didnt get effective.Thank to hansd empty project I manage to begin my project and conceive my GUI:https://community.st.com/s/question/0D50X0000AntXX2SQM/simpliest-ide-to-con...

0690X000008BgXXQA0.png 0690X000008Bf53QAC.jpg

Set values of LTDC Timing for stm32f429ZI

HelloI have a TFT_LCD 5.7 inch. I want start up it with STM32F429Discovery but I have a problem according to the LCD datasheet I have to set Vsync (Front-Porch) = 4.5 TH (Hsync Period).But I can't give float numbers to the LTDC registers. LCD datash...

Somid.16 by Associate
  • 2179 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.