STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Adding text while working

Hello!I work with textArea.I want to add new text while program working. For example - I get array of filenames and I want to put filenames to screen (and later select one of them by touching).How can I do this? How to create new textArea while pro...

EEuge by Senior
  • 1964 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFX violates global namespace standard

All declarations in the global namespace that start with an underscore are reserved by the C++ compiler according to the C++ standard. See: https://en.cppreference.com/w/cpp/keyword TouchGFX violates this by converting any images to "_filename" and ...

j o by Associate II
  • 1887 Views
  • 3 replies
  • 0 kudos

I am using a touchgfx scrollable container to create a list. I include a radio button in the container. My problem is: In the container the radio button is assigned to radioButtonGroup1.

When I select the radio button for a list element, the other list element radio buttons are not deselected. Is there a way to make the radiobuttongroup for all of the list elements the same?

MLync.1 by Associate II
  • 910 Views
  • 1 replies
  • 0 kudos

Transmit buffer generated by HAL_DCMI_Start_DMA over UART interface in Snapshot mode of low-resolution image

Can I transfer buffer generated HAL_DCMI_Start_DMA through UART interface. I am using STM32f4 discovery board. My UART stop working after HAL_DCMI_Start_DMA call. My main function is attached. int main(void){ /* USER CODE BEGIN 1 */ OV9655_IDTypeDef ...

Junaid by Associate II
  • 1113 Views
  • 1 replies
  • 0 kudos

MJPEG Parse Error

Hi,​I am using MJPEG from Official Source Code, and when I parse the AVI that always come out HardFault Information at Video format parsing.​Code is official , AVI is too.​I am not sure about is the buffer size enough to storage the total file and de...

0690X00000DBl2DQAT.png 0690X00000DBl2cQAD.png

Resolved! COPY and PASTE between files?

Has this function been provided? I would love to have the function of copy and paste between two files, so I donnot have to create those same screens again in a new file.:grinning_face_with_sweat: Br,Devin

WDAI.1 by Associate II
  • 2044 Views
  • 3 replies
  • 0 kudos

Resolved! "Virus" found in TouchGFX Designer 4.10.0

I have posted this in zendesk, but am then referred to ST Community. I would like to re-post here, so that someone in ST can help to follow up.====================================We have a project running on TouchGFX 4.9.3, and we have just tried to ...

S.P. by Associate II
  • 7555 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.