STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Zendesk vs ST website for TouchGFX support?

What is difference between being a member of st.com and touchgfx.zendesk.com?When I click community in Zendesk, I end up at st? Why should I not just log in to st?What does Zendesk give me that ST does not?

JOsen by Associate III
  • 1279 Views
  • 1 replies
  • 0 kudos

touchgfx with spi lcd

I arange the all settings acroding to information on https://touchgfx.zendesk.com/hc/en-us/articles/203642951-MCUs-without-TFT-controllerand when I try to debug my software on my custom board it says "can not execute Mi commands load ..."when I comme...

KERDO.1 by Associate II
  • 2017 Views
  • 5 replies
  • 0 kudos

Problem with interface with physical buttons

Hello!I try to create intefrace with physical buttons, following this instruction https://touchgfx.zendesk.com/hc/en-us/articles/205074551-Interfacing-with-physical-buttonsI Added  ../Middlewares/ST/touchgfx/framework/include/platform/driver/button...

EEuge by Senior
  • 3527 Views
  • 9 replies
  • 0 kudos

STM32F7 + USB HS +Touchgfx +FreeRTOS

Hello ST Team,I am working on USB HS HID Device only along with touchgfx +FreeRTOS in STM32F7 controller.But creates reading & writing Issue when touchgfx is included.I have even checked the clock but no use. 48Mhz is clock its proper.Any help would...

Uc.2361 by Associate II
  • 2756 Views
  • 5 replies
  • 0 kudos

Resolved! CubeMX 5.5.0 + Touch GFX Designer 4.13: GUI can run without freeRTOS on own HW STM32F429\439 TFT RGB 16bit LTDC?

Hi, I have my own hardware that run without freeRTOS on STM32F429 with STemWin GUI.In the revision hw I'm evaluation to use UI based on Touch GFX latest ver 4.13 + CubeMX 5.5.0.Can I migrate my full application without use freeRTOS with Touch GFX UI?...

stm32l4R9 eval board demo firmware

Hello In my touchgfx project , I have to do some power consumption works. I know there is a demo firmware for stm32L4R9 evel board. I want to take a look at clock configurations and chrom art accelerator enabling/disabling functions but I cant find...

Epamuk by Associate III
  • 1484 Views
  • 3 replies
  • 0 kudos

Gauge Image only half appearing on screen, it simulates ok on ToughGFX designer and also with visual studio.

i have use example from TouchGFX Demo 1, ive gone through code but cant see anything obvious. with the 746 Disco board, above.i set up the project through TouchGFX designer, only one screen and copied code from example, here is the view.cpp i have c...

0690X00000D9vIlQAJ.jpg
BO Re.1 by Associate II
  • 2828 Views
  • 8 replies
  • 0 kudos

Resolved! Various screens vs various containers

Hello,If various elements of the GUI I'm working on are going to be shared amongst most of the screens (footer, header, status bar,…), do you think it's a good idea to use a single TouchGFX screen and to change only the central content by means of co...

GMeur by Senior II
  • 1113 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.