STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Windows PC Simulation crashes when using a single widget (Button). Works fine with no widgets (only hard-coded text). Help!

Windows PC Simulation crashes when using a single widget (Button). Works fine with no widgets (only hard-coded text). Help!Everything works fine when using TouchGFX Designer to run a simulation on a Windows PC. But we are trying to build everything w...

VSimu.1 by Associate III
  • 3029 Views
  • 7 replies
  • 0 kudos

do you have another solution for us

We are using stm32H743We need a frame buffer of 150K to our LCD. we do not have an external RAM, so we use the 412K internal RAM.We also work with USB (Full speed mode).each peripheral work on it own , but not together. if we enable both of them they...

Hmizr.1 by Associate II
  • 1311 Views
  • 1 replies
  • 0 kudos

Resolved! Animated images with thousands of .PNGs slows down a TouchGFX Designer. Looking for alternative approaches.

Hello, I’m working on device equipped with STM32H753 and LCD (320x240), 16 MiB of SDRAM (available for caching will be about 13 MiB) and SD card (SDMMC interface) that will be used also for storing images for TouchGFX.In some cases device shall disp...

scott.sp by Associate II
  • 2082 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.