STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

spurious touchs on spi display

When i the touchscreen on my LCD it occassionally presses somewhere else on the screen to where i have pressed.The simulation on touchgfx works perfectly which means it isnt the code ive implemente in the virtual functions. Only assumption is that th...

MikeP by Senior
  • 1809 Views
  • 2 replies
  • 0 kudos

"Load images into target memory"

Hello, I am trying this example to use LCD_HDMI from STM32Cube repository.Board: STM32H747I-DISCOToolchain: STM32CubeIDESTM32Cube_FW_H7_V1.7.0\Projects\STM32H747I-DISCO\Examples\LCD_DSI\LCD_DSI_VideoMode_DoubleBufferingI am following the guidelines i...

Sayali by Associate II
  • 3696 Views
  • 5 replies
  • 1 kudos

Resolved! Adjusting frame rate fps of display for TouchGFX

Hello everyone, I am trying to adjust the frame rate(to a lower fps) of the display on STM32F429i discovery board. I saw from this manual cd00278141-qvga-tftlcd-direct-drive-using-the-stm32f10xx-fsmc-peripheral-stmicroelectronics.pdf saying there's a...

0693W000001sH0oQAE.png
HPam.1 by Associate II
  • 4642 Views
  • 3 replies
  • 0 kudos

Resolved! Can I change the text rendering?

I want to make a TextBox with a cursor (caret) and would like to change the TextAreaWithOneWildcard. Where can I see the implementation of the draw method? Is this code open?

MWate.1 by Associate II
  • 2549 Views
  • 4 replies
  • 1 kudos

stm32cubeIde 1.3.1 and touchgfx 4.13.0

Hi.I have a project with stm32cubeIde 1.3.1 and touchgfx 4.13.0 as was described in "STM32CubeIDE 1.2.1 and TouchGFX 4.13.0 with STM32F746G-DISC0 kit" video on youtube that Jan 30, 2020 - Uploaded by EE by Karl. https://www.youtube.com/watch?v=12KXre...

Mvona.1 by Associate II
  • 4493 Views
  • 6 replies
  • 0 kudos

Resolved! Can I ask GFX designer to allow some warnings?

H​iGFX's designer tell me that all warnings would be treated as errors.But it's part of the LibJPG library, and I can't change it.Is there any way to get rid of this "error"?​I want to open a JPG image in the simulator and display itThank you very mu...

0693W000001ruB0QAI.png
Korry by Associate III
  • 1827 Views
  • 3 replies
  • 0 kudos

Text configuration in VisualStudio

HiIn the TouchGFX Designer is it possible to set the text configuration to "Remap texts" and "A4" and it works well when I'm generating the code. But when I build within VisualStudio these settings will not applied, even they are added within the "ap...

Marco.R by Senior
  • 1786 Views
  • 3 replies
  • 0 kudos

how to fix the [makefile:94: touch.elf] Error 1

I saw a guy on youtube doing project on disco board. So I though I would give a try myself I got latest CubeIDE and Touch GFX I am using 32F469I Discovery but I am getting this error[makefile:94: touch.elf] Error 1touch.elf section `ExtFlashSection' ...

MNapi by Senior III
  • 3363 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.