STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Graph or Scope, how to ?

Hello,I'm working on a quick and dirty prototype for thermal regulation.It's the first time I use TouchGFX (but I'm quite used to STM32s for like 10+ years, ST partner, etc.).The UI is very simple (one screen) and runs on a F469 discovery board, I us...

Resolved! Warning/error in ButtonWithIcon

Version:TouchGFX 4.13.0File:touchgfx\framework\source\touchgfx\widgets\ButtonWithIcon.cpp:39The code is:#ifdef __IAR_SYSTEMS_ICC__ // Only include in IAR compilation #pragma diag_suppress=Pe997 // Suppress warning for intentional virtual function ov...

SZano by Associate III
  • 1208 Views
  • 2 replies
  • 0 kudos

TouchGFX custom driver- vsync problem

Hello,I want to run TouchGFX on STM32F413VGTX MCU. It Doesnt not have LTDC nor DMA2D so I want to make it run using FSMC without graphic accelerator with my ST7529 LCD controller. The problem is I can not make it run.I created a project with ToucGFX ...

0693W000001s14uQAA.png
maciek by Associate II
  • 3476 Views
  • 4 replies
  • 0 kudos

STM32F7508-DK: Can I use an external LC display?

Good morning (o;Thinking of getting me the F750 discovery kit as it features an internal LCD controller...Now...can I disconnect the supplied LC display and attach an external LC display to it via the IO headers?Would it be possible to drive a RGB 72...

Davorin by Senior
  • 1364 Views
  • 1 replies
  • 0 kudos

How to get current screen

My application has many screens, after idle for some time, I need to show a advertisement screen.I want to implement it something like Modal dialog box to cover the whole current screen. So I need to get the current active screen, actually a containe...

shark by Senior
  • 2254 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.