STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Dynamic vector in custom container

Hello.I'm trying to create custom container with any number of elements.I created custom container which contains Scrollable Container and List Layout.I want to dynamically add elements to List Layout. Elements are simple containers which contains te...

Example codes give error.

Hi,When I want to run a touchgfx example (of demo) in designer, compiler give me error like follows.Run Simulator Generate Done Generate Assets make -f simulator/gcc/Makefile assets -j8 cannot load such file -- lib/emi...

The button pressed animation is displayed but the callback is not executed every time the button is clicked

Hi everyone,I am a student and I am working on a project involving an STM32f429ZI and a 7inch touch display.It's the first time I work with displays, I am trying to create a GUI using touchgfx.I have been working on it for a week now and so far I man...

Touftoufe by Associate II
  • 2212 Views
  • 4 replies
  • 0 kudos

F429 TouchGFX not working on own PCB

Hi! I have a program with TOUCHGFX running on F429-DISC1. It works fine and display correctly both on the disc1 original touch screen and an external screen with RGB666 interface i connected to the header.​As it look alright on the DISC1 board, i mov...

Resolved! System Requirement for TouchGFX on STM32F303xx

I am using STM32F303VBT6 in my application where I need to use the graphical library for advanced HMI development. The system would have more than 15 screens (consists of Text, symbols, images etc.), LCD is not a touch display it is simple 262K color...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.