STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX with DSI Video mode

Dear ST Team,I'm doing a project about: display LCD (DSI Video mode) with TouchGFX. I have example TouchGFX DSI Adapted CMD mode, but can't find out example for DSI video mode.Please give me some idea!!!Thanks

NHo.1 by Associate III
  • 2441 Views
  • 3 replies
  • 0 kudos

Touchgfx DSI Video Mode - LTDC Overflow

We are running into some issues getting Touchgfx with DSI Video Mode Running1. uC - STM32F779BI2. Display - 720 *12803. Display Controller - ST77034. No of MIPI Lanes - 2 lanes5. DSI Host Mode - Video Mode6. RGB 565We have been able to communicate wi...

SNare.1 by Associate
  • 4228 Views
  • 7 replies
  • 0 kudos

Issue with Changing Pixel Format on STM32F769i

I followed this guide to changing the pixel format of an application. Although my TouchGFX designer file does not have the code listed above the framebuffer pixel format table 2/3 of the way down the page, in the Designer itself it reports 16bit colo...

0693W000001qYBuQAM.png

Resolved! Box / Border for Textarea

HiOur marketing needs to know how much space they have for translation etc. and requested if we can show this visually on the screens. The easiest would be if each textarea had a box or border, which indicates the size.Is there an easy way to add a b...

Marco.R by Senior
  • 1711 Views
  • 1 replies
  • 0 kudos

Resolved! alternative to TICK_INTERVAL_MS constant in touchFGX

Hello,I'm wondering if there is a an alternative to TICK_INTERVAL_MS constant which is deprecated. It is said that handleTickEvent() function is called by the Application on the current screen with a frequency of Application::TICK_INTERVAL_MS.For the...

AJT141 by Associate III
  • 3071 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX source code

Hi,I am working on a project where using external bin lib files is forbidden for safety and security reasons. Is the TouchGFX source code available ? Do we need to buy a license or something like that ?Thanks,Olivier

STMF469I DISCO TouchGFX demo problem

Hi,I have compiled and load the demo to the board with STMCubeIDE 1.4.0 on Linux.When I start the board, it seems that the display is correct during a quarter of second or less.Then the colors are getting weird, like if there is a palette problem.Doe...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.