2020-10-30 1:33 AM
Hi,
I have compiled and load the demo to the board with STMCubeIDE 1.4.0 on Linux.
When I start the board, it seems that the display is correct during a quarter of second or less.
Then the colors are getting weird, like if there is a palette problem.
Does anyone have the same problem?
Thanks,
Olivier
2020-10-30 1:41 AM
Hi,
Please provide more details. Images, videos would be great.
Thanks!
/Martin
2020-10-30 2:12 AM
2020-10-30 4:13 AM
Looks like, among other things, the external flash hasn't been programmed with any images. Can you verify?
2020-10-30 4:49 AM
First thanks for your help !
I am more a vim/emacs makefile guy, so I am not comfortable with ide ...
After the "build", I press "run". I get this on the console:
STMicroelectronics ST-LINK GDB server. Version 5.6.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0-RC1
-------------------------------------------------------------------
ST-LINK SN : 066FFF303435554157031815
ST-LINK FW : V2J37M26
Board : 32F469IDISCOVERY
Voltage : 3.25V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x434
Revision ID : Rev A
Device name : STM32F469xx/F467xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_OQR02D.srec
File : ST-LINK_GDB_server_OQR02D.srec
Size : 234112 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 5]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:04.820
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
Should I do something else ?
2020-10-30 5:11 AM
Nothing in there says anything about programming the external flash (starts at 0x90000000)
Can you try choosing the right flash loader in CubeProgrammer? Try using the stand alone CubeProgrammer application.
2020-11-01 7:24 AM
2020-11-01 7:25 AM
2020-11-01 8:53 AM
For your info, I have done the same thing with the TouchGFX demo for the STM32F769I Disco and it works well !
So my setup seems ok.
2020-11-02 11:59 PM
Hello,
Can you send your project ? It will be easier if we test on our side.
Please remove all unnecessary folders like the build folder in TouchGFX/ folder and touchgfx middleware folder so that your project is not too large.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.