STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

CircleProgress: PainterRGB565Bitmap::render() crash

Hello,I implemented the demo animation described in the CircleProgress example.Everything works correctly with the simulator.On the target, a crash occurs after calling the circleProgress.setValue (nextValue).The crash occurs even if the initial valu...

ALomb by Senior
  • 2954 Views
  • 3 replies
  • 0 kudos

Resolved! Example supplied creates 2GB extflash.bin file

Hi,I am trying out the following tutorial: https://support.touchgfx.com/docs/tutorials/tutorial-01, which is very basic.In the "Running an Example on an STM32 Evaluation Kit" section, when pressing run target, everything compiles, the MCU is loaded, ...

Port TouchGFX to FMC with ILI9341

Hello,I developed a STemwin project a few years ago, with an STM32F437 and an LCD(320x240) driven in FMC with the ILI9341 controller.I am looking to migrate this card to touchGFX for a different application. But I have an issue:If the screen is stati...

0693W000006G9c5QAC.png
PCu1 by Senior
  • 2224 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX - STM32H747 Discovery "Error external loader cannot be loaded", this problem might conduct to "failed download Segment[2]"

Hello everyone,I have a STM32H747I-DISCO and I am trying to use it with TouchGFX in the first part. But the problem is I cannot use it directly with TouchGFX "Run Target" mode.I have few errors, I tried to run as admin but it didn't work. I have the ...

0693W000006H8WIQA0.jpg 0693W000006H8WDQA0.jpg
SEmar by Associate II
  • 1847 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.