STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Control Pins and communicate via usart issue

Helleo,I am newbie in Touchgfx and I try developing first project. I am willing to data transfer stm32746 to pc via usart and control pins.When I click the button stm doesnt send data via usart or stm doesnt control pins.Screen1View.cpp codes:#includ...

0693W000006GtqXQAS.png
FLine.1 by Associate II
  • 9292 Views
  • 22 replies
  • 0 kudos

Resolved! China texts

Hello!I have a typography, which contains this set of symbols "0-9,A-z,�?-�?,0x20-0x7F,0x401,0x451"But I want to use China and Japan languages.In TouchGFXDesigner all OKBut in application - "????"How to fix?

0693W000006HOdPQAW.png
EEuge by Senior
  • 5635 Views
  • 11 replies
  • 0 kudos

Resolved! Problem with text wildcard

Hello! I have textArea with wildcard, which is updated by Slider movingvoid OPTIONS_SCREENView::R_Slider_MOVED(int value) { RGB_LED_Sample_box.setColor(touchgfx::Color::getColorFrom24BitRGB(R_Slider.getValue(), G_Slider.getValue(), B_Slider.getValu...

EEuge by Senior
  • 2819 Views
  • 6 replies
  • 0 kudos

TouchGFX show

I write well void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect).But there's something wrong with the display.I want a red background, but I want a white background on the screen.void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rec...

张成.1 by Associate
  • 1322 Views
  • 1 replies
  • 0 kudos

STM32F746 Display getting stuck

Hello, I am using STM32F746 with FMC SDRAM, QSPI flash, DMA2D. I observed my display get stuck like below image after some time. When I reset disp pin of display (out of 40 pin) , it starts working again. I am not able to find out issue. Any suggesti...

0693W000006HPBqQAO.jpg

Central text alignment doesn't work

 void SmallFlag_Container::SetLanguage(Bitmap icon, TEXTS lang) { FlagImage.setBitmap(icon); LangText.setTypedText(TypedText(lang)); // LangText.resizeToCurrentTextWithAlignment(); LangText.invalidate(); }In TouchGFX all is right but in r...

0693W000006HKJkQAO.png 0693W000006HKK9QAO.png
EEuge by Senior
  • 1350 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.