STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Histogram Graph, edit a single value

Hi all,How is it possible to change a particular index of Histogram graph?I would like to change item n°2 (see the picture) from a start to a final Value, without redraw entire graph.Second question, Is it possibile to change the colour of a single i...

MPast.1 by Senior II
  • 942 Views
  • 0 replies
  • 0 kudos

Resolved! How to scroll a scrollist?

Hello!A have a window, his height is 10 strings. Scrollist have 30 strings.When I add 11-30 strings, they are out of window. I can manually scroll list to last element.How can I do it by software?Something like ScrollList1.ScrollTo(25);.....

EEuge by Senior
  • 1638 Views
  • 1 replies
  • 0 kudos

STM32F7: Ram needed for a 800x480 24bit display.

Dear All,I'm approaching for the first time STM32F7 family. My need is to use this microcontroller essentially to drive an 800x480 TFT LCD 24 bit. It's the first time that I'm doing it.Reading online the RAM needed for a similar resolution is 800*480...

MDell.1 by Associate II
  • 2555 Views
  • 3 replies
  • 0 kudos

Resolved! Reset Graph X Values

I'm using the dynamic graph to represent a small dataset. The data is acquired all at once through a back-end process, leaving me with an array of around 1000 datapoints. Once acquisition is complete, I use the following code to refresh the graph.gra...

Disable external flash programming

Hello dear engineers,How can I instruct the STM32cubeIDE to neglect programming of the exteranl flash parts?This parts have been placed in an external ram memory which is to be read and programmed in runtime.In Keil ide, it simply says since no flash...

Resolved! What is typical development flow for TouchGFX?

So I developing prototype using STM32F769 Discovery Kit. At first I develop the UI using TouchGFX and so far so good.But I realize the generated codes from TouchGFX does not really generate driver code for other component e.g. Virtual Component Port....

BParh.1 by Senior III
  • 5252 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.