STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32H board with LCD screen and MCU DAC outputs

Hello,I am new to the discovery line up.I am looking for a ST32H board with fast direct MCU connection LCD similar to the STM32H745-DISCO with 2 MCU DAC outputs. I can't use the codec DAC because the latency is too long. I see only one DAC connected ...

FEory.1 by Associate
  • 1065 Views
  • 0 replies
  • 0 kudos

OSWrappers::signalVSync hangs

Hello!I made the project for a custom SPI display with configuration like screenshot below: Added in main.c:void StartDefaultTask(void const * argument) { /* USER CODE BEGIN 5 */ MX_TouchGFX_Process(); /* Infinite loop */ for(;;) { osDe...

0693W00000AMtNOQA1.png
Vitaliy69 by Associate II
  • 2379 Views
  • 5 replies
  • 0 kudos

Resolved! Package Server can not be reached 4.12.3

Hi,I have started using touchgfx recently and am having trouble accessing examples. When I open the designer I am able to see my applications and online applications, but I cannot access the example UI's nor can I access any online applications.I get...

belair55 by Associate III
  • 3806 Views
  • 10 replies
  • 0 kudos

Resolved! STM32446E-EVA DCMI

Good morning.I am using the STM32446E-EVA board.I want to read data about video from CAMERA through serialI am not sure where it is because it is the DMA part.In order to read CAMERA data, which function part can we know by reading the value in part?...

LSang.11 by Associate II
  • 1378 Views
  • 1 replies
  • 0 kudos

The LCD refresh rate on H7 slower than F4

I use FMC for both H745ZI and F427ZI. I already configured all cores to run at the same clock (168Mhz), but write buffer to F4 seen faster than in H7.Anyone can help me solve this issue? I have included clip at: https://drive.google.com/file/d/15hbrx...

HNguy.21 by Associate II
  • 2856 Views
  • 6 replies
  • 0 kudos

1-Kbyte boundary cross problem, LTDC 1k Boundary

Hello,We are struggling to implement the 1k boundary when reading/writing to a frame buffer i.e. to avoid read operation being split into single accessesHow to do this is described in the application note here:https://www.st.com/resource/en/applicati...

VSimu.1 by Associate III
  • 959 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.