STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32H745I-DISCO HMI PROBLEM

Hello, I have STM32H745I-DISCO and TouchGFX 4.16.1 Designer. As I understand it, TouchGFX does not support the board in my hand. How can I control my HMI? Is there software that supports this card?

aşahb.1 by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

Resolved! Is Graph "Precision" relevant when using float?

Hi,I am trying to understand the graph "precision" as explained here:https://support.touchgfx.com/docs/development/ui-development/ui-components/miscellaneous/dynamic-graph#precision"If for example the level of precision is set to 0.1, each data point...

STM32L4R5AIIx, DCMI and MT9M114 camera chip. DMA does not receive request that there is data in the DCMI data buffer.

I have been working for about 4 weeks on a project which has the STM32L4R5AIIx processorand is using the camera MT9M114 from ON Semiconductor.The project uses the following command to take a snap shot."HYPERRAM_BASE_ADDRESS" is the starting address o...

KNguy.5 by Associate
  • 871 Views
  • 0 replies
  • 0 kudos

LIBJPEG Question

Hello, I am trying to implement bmp to jpeg encode application. I have used official STM code example. There is no compile error.I gather RGB565 data from OV7670 camera. I can successfully write to SD card as 16 bit bitmap file and open it on a Windo...

In STM32F429 Software struct in backPorchExited().

Hi,Created one simple application in TouchGFX for STM32F429 Disco board. But it struct in backPorchExited() void TouchGFXHAL::taskEntry(){  enableLCDControllerInterrupt();  enableInterrupts();  OSWrappers::waitForVSync();  backPorchExited();  LCD_IO...

MAaru.1 by Associate II
  • 1056 Views
  • 1 replies
  • 0 kudos

Resolved! printing a string

Hi, I'm trying to print the string. What is that I'm missing?This is my func : void Screen1View::UpdateWildcardTexts(char* a) { Unicode::snprintf(textArea1Buffer,10,"%s",a); textArea1.invalidate(); }This is how I test it :void Screen1View::setupSc...

Ezgi by Senior
  • 2003 Views
  • 2 replies
  • 0 kudos

CubeMX 5.0.1 + STemWin on STM32F769-DISCO

Hello, does anyone have an *.ioc file or give me the right settings to create a project with CubeMX without using BSP files. Everything is in CubeMX, so integrating BSP files is not needed anymore.I'm struggling with the display settings, concerning ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.