STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

About the image size

I have tried to use RGB565 format to store images, the size is too big.Then I used L8_RGB565 format, the size is reduced by nearly half, but it didn't feel good enough.L8_RGB565 image is divided into two pieces of data: pixels and CLUT. I think the C...

V.H by Senior
  • 1043 Views
  • 1 replies
  • 1 kudos

IS there a graphics engine for STM32H475 available?

Hi, I'm new to this board. I've decided to switch from ATMEL to STM µControllers after Microchip bought ATMEL and apparently decided to phase out ATMEL Studio.I bought the STM32H745 Discovery board assuming TouchGFX would be working on it. However, a...

Hansel by Senior
  • 1180 Views
  • 3 replies
  • 0 kudos

Break at IS_TIM_SLAVE_INSTANCE when debugging

Hello,I've been trying to program a GUI application using Touch GFX with a custom board including a STM32F469II. Recently however, the program has begun to act weird when I try to debug it and fails before I have to restart it manually. Here what I c...

TDele.1 by Associate III
  • 2674 Views
  • 3 replies
  • 0 kudos

Resolved! DMA2D throws configuration error

Hello!We are use STM32H747 and TouchGFX. We are need to use DMA2D. But we have issue with mode DMA2D_R2M.Our configuration hdma2d.Instance = DMA2D; hdma2d.Init.Mode = DMA2D_R2M; hdma2d.Init.ColorMode = DMA2D_OUTPUT_ARGB8888; hdma2d.Init.Output...

VLesc.1 by Associate
  • 1710 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.