STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Why the Dynamic Graph On the LCD is flickering?

Hi,I have a problem with Dynamic graph on the LCD that when I upload the code, the graph on the screen start to flicker but it's not the in the simulation. I shared the video below.I want to Update 680 data points on the Graph every tick in "handleT...

ATavo.1 by Associate III
  • 4502 Views
  • 8 replies
  • 0 kudos

Working with touchGFX in a team

We have a pretty big project and we want 2 people to develop screens for one project. we are using bitbucket as a repo and the idea is person 1 can make there screens on a branch and person 2 can make theirs on a separate branch. The merge them at ...

jeff belz by Associate II
  • 1619 Views
  • 1 replies
  • 0 kudos

[TouchGFX] Using Camera with TouchGFX GUI

Hello, I'm using TouchGFX with STM32F746NG Discovery Kit.Now I want to create an widget (or something like that) in TouchGFX where I can stream data from Camera which connected with STM32F7 kit. I have read TouchGFX documents but it's seem no object ...

FrontendHeap problem

Hi ,I have problem with the Heap issue (for many views I think)I try to comment some view in FrontendHeapBase and it can flash into kit, but I found out in some view using more heap than declare --> it errors.Can you help me fix this problem??Thank a...

HNguy.21 by Associate II
  • 6672 Views
  • 13 replies
  • 0 kudos

I am trying to build a GUI to display a chart for STM32's ADC converted values, ; the code works fine before without touchgfx, but when i configure Touchgfx I generated the code from the application , then build the project, i get errors as whown below:

../TouchGFX/target/generated/TouchGFXConfiguration.cpp:17:10: fatal error: texts/TypedTextDatabase.hpp: No such file or directory fatal error: touchgfx/hal/GPIO.hpp: No such file or directory make: *** [TouchGFX/target/generated/subdir.mk:28: TouchG...

Zbena.1 by Associate II
  • 3204 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.