STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX X-Nucleo GFX01M1 integrate hardware button.

I´m usiing TouchGFX with X-Nucleo GFX01M1Being a beginner I would as a first step to change the screen with the joystick on the board.Checking an example I notiiced that the Action is set as:and the interacion is set as with Run Simulation i could ma...

0693W00000JNrFzQAL.png 0693W00000JNrG4QAL.png 0693W00000JNrGEQA1.png 0693W00000JNrG9QAL.png
FTrom by Associate II
  • 2041 Views
  • 3 replies
  • 0 kudos

Tick Rate Slows to 1 Tick per 2.5 Seconds

I am working with a project in TouchGFX Designer/Generator 4.17 and STM32CubeIDE 1.7.0, which uses the LTDC interrupt from the display to drive the main display loop. The display is configured according to the manufacturer's specifications, and Touch...

DSwea.1 by Associate III
  • 4544 Views
  • 8 replies
  • 0 kudos

STM32 OV7670 VIA DCMI

Hi, for a few days I have been trying to run the OV7670 camera on the STM32F446RE (Nucleo), but the image it gets does not resemble what the camera is looking at, I have checked the connections many times, but I have not found any problem there, mayb...

ERych.1 by Associate
  • 1703 Views
  • 0 replies
  • 0 kudos

BSP LED driver for STM32H747I-Disco board

Can somebody send me a template application which contains BSP (Not STemWin) definitions for using LCD display? I just would like to show very basic progress bar, text.Then can anybody tell me how can I rename a project?Many thanks for your help.Loui...

Louie88 by Senior II
  • 2122 Views
  • 3 replies
  • 0 kudos

How to make STM32L476VGTx use GUIBuilder?

HelloI want to know how to make The STM32L476VGTx can use GUIBuilder to design a custom GUI to display on an LCD screen.I want to know if it is possible or not. or is there any way(Actually my project is a ST25R3916 board that uses an STM32L476VGTx M...

mchal.11 by Associate
  • 1210 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.