STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Force LTR text orientation

Hi all,I am struggling how to force a LTR text direction from a certain point onwards. For example in the image the version is written backwards as the first text has a RTL direction. I saw that it exists a specific LTR Marker with a code U+200E but ...

0693W00000KboqfQAB.png
MKsen.1 by Associate II
  • 2248 Views
  • 2 replies
  • 0 kudos

TouchGFX: Trouble migrating from 4.16.1 to 4.17.0

I'm having some troubles migrating a project from 4.16.1 to 4.17.1.My board is NUCLEO-H743ZIWhen linking a project after migration i get some errors like:"undefined reference to `touchgfx::TextArea::setTypedText("This error come from some auto-genera...

Roberto C by Associate III
  • 2018 Views
  • 3 replies
  • 0 kudos

MIPI-DSI Amoled LCD

Hi,I am trying to drive 454*454 px amoled lcd with stm32l4r9 mcu and the image cannot be displayed properly. I am using the cubemx settings and the desired settings according to lcd datasheet. Any advise ? 

0693W00000KbvMNQAZ.png 0693W00000KbvMXQAZ.png
er3481 by Senior
  • 2522 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX 4.18.1 - generated file build error

I recently upgraded my project from 4.16.1 to 4.18.1. After integrating the designer files in to my project build environment, I am facing build error with a designer generated file. See attachment. Obviously I cannot modify the generated files to a...

0693W00000Kbkr5QAB.png
BGuth.1 by Senior
  • 1211 Views
  • 1 replies
  • 0 kudos

Flickering on STM32H755 with alpha effects on images

Hi everyone,I have the following "flickering" problem using TouchGFX with an STM32H755 board. The problem occurs when performing a "fade in" effect by varying the alpha of an image from 0 to 255 in a certain time.Everything else seems to work fine, b...

0693W00000Kb8uaQAB.png 0693W00000Kb8v4QAB.png 0693W00000Kb8vdQAB.png 0693W00000Kb8vxQAB.png
FBena.1 by Associate II
  • 3224 Views
  • 5 replies
  • 1 kudos

Resolved! Error with TouchGFX conversion from 4.17.0 to 4.18.1

My TouchGFX project is originally created with v4.16.1. I just downloaded latest version of TouchGFX i.e. 4.18.1. The latest version tried to convert my project and threw below error. So, I opened the project with v4.17.1 and it converted fine. But w...

0693W00000JN7Y3QAL.png
BGuth.1 by Senior
  • 2823 Views
  • 6 replies
  • 0 kudos

Resolved! How to know if an image is used in TouchGFX

A lot of images are uploaded in to my TouchGFX project. I would like to removed unused images from there. How would I know if a particular image is used in the project or not? For example, Texts -> Typographies tab shows how many uses a particular fo...

BGuth.1 by Senior
  • 2787 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.