STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32G431 Board is missing

Hello,I've recently bought X-NUCLEO-GFX01M2 expansion for STM32G431 evalboard. And while I was trying to create my first project I've noticed it does not offer any Project for this type of board. On the ST page there is a discription, that mentiones ...

Is it possible to rotate image group where multiple images are overlaid using Touchgfx texture mapper feature?

Hello, when I check the rotation feature on touchgfx library, I could find texture mapper feature to rotate images. and I think I can test it uisng texture mapping example from touchgfx-designer. But this example is just rotating each image. What I w...

Tiel by Associate II
  • 3684 Views
  • 1 replies
  • 0 kudos

Resolved! Cube IDE - Long Loading Time with Graphics.

Hi,When debugging with Cube IDE programs without any TouchGFX graphics load quickly using the debugger typically 20 to 30 seconds. When TouchGFX is used such that the NOR Quad SPI Flash has to load the loading time can easily exceed 3 minutes. With ...

TouchGFX GUI with another project

Hello,Is it possible to use the GUI developed with TouchGFX of a project for another project but with another STM32 board? Please help me with the steps to follow in order to use the graphical interface developed with STM32G071 in another board.Thank...

TSour.1 by Associate II
  • 2380 Views
  • 3 replies
  • 0 kudos

STM32H747 Hardware JPEG Compatibility issue

Dear all, I have successfully implemented the example STM32CubeH7-master\Projects\STM32H747I-DISCO\Examples\JPEG\JPEG_DecodingFromFLASH_DMA with the image file given as C source there.Now I wanted to change the image data, which however was not succe...

0693W00000D0BIXQA3.jpg 0693W00000D0BGYQA3.jpg 0693W00000D0BJGQA3.jpg 0693W00000D0BJQQA3.jpg
SFuch.1 by Associate III
  • 2700 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.