STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

interaction in button in touchgfx not work

I have setting a button with it's interactionWhen I touch the button is detected (the picture of it changes) but the interaction of the button (calling function) not worksI tested in keil and stm32cubeide but the problem doesn't solvedcan everybody h...

jhasa.2 by Associate III
  • 1898 Views
  • 3 replies
  • 0 kudos

TouchGFX - reducing flash consumption

Hi,I am trying to implement simple GUI with TouchGFX 4.20 on STM32F303 MCU. I have limited amount of memory for GUI. Even few kBytes important. When I look memory consumption of TouchGFX I see weird functions that I don't call or not to use some widg...

0693W00000SvmQmQAJ.png
SSone.1 by Associate III
  • 1652 Views
  • 1 replies
  • 1 kudos

When I enabled DWT (STM32F407), for getting microsecond delays, everything works fine but suddenly all activity comes to a stop for about 2 minutes and then everything starts working as usual. Interrupts seem to be occurring but everything else freezes.

This happens at randomly. Spent more than a month trying to figure out the issue and never suspected DWT. When I commented out DWT everything works fine now. Can someone educate me on why this is happening and how to avoid it? Thank you for your time...

"genlock" and the STM32H7 LTDC

I am trying to use the STM32H723 as a video output (tying the LTDC pins to an ADV7115 to convert them to HDMI). The idea is to read the bus traffic of an old 8-bit computer and generate the display from that traffic (as part of other duties). My conc...

Deleted Screens are not completely deleted

When I delete a Screen in TouchGFX Designer, the screen is deleted in the designer and the base files are also deleted. But the view and presenter files are not deleted. When I delete my user code in view and presenter, then these files are indeed de...

Pirol by Associate III
  • 3662 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.