STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Why can't get adress of 2x16 LCD in Cube IDE?

Hi every one. I am using STM32-F401RE, 2x16 LCD with I2C integrate, i connect SCL-SDA-Vcc and GND each other (board and LCD), i tried to make scann program to know adress of LCD in this way:#include "main.h"#include "stdio.h"I2C_HandleTypeDef hi2c1;U...

SMusc.1 by Senior
  • 13476 Views
  • 10 replies
  • 0 kudos

Resolved! undeclared (first use in this function)...

Hello, I am going crazy, I always get the error that the structure Lcd_Ctx is not declared, while it is clearly declared (by including "stm32h750b_discovery_lcd.h"). With F3 I can find the structure declaration.If I change the file from .c to .cpp th...

0693W00000UoQm6QAF.png
pk84 by Senior
  • 16142 Views
  • 18 replies
  • 0 kudos

Why does model::tick() not getting called?

I found out that LTDC interupt callback is not getting called but can't figure why. Following code is auto generated by CubeMX LTDC interrupt is enabled in NVIC."TouchGFXGeneratedHAL.cpp"extern "C" { void HAL_LTDC_LineEventCallback(LTDC_HandleTyp...

0693W00000UnC2bQAF.png
manto.1 by Senior
  • 1317 Views
  • 1 replies
  • 0 kudos

Scrollable text

Hello, Is it possible to know scrollable text coordinate? I want to do editable text in keyboard and by touch I know where the cursor needs to be. When I touch somewhere in the text I know touch coordinate but I need to know scrollable text coordinat...

heyo by Senior
  • 1438 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX: How to enable an external data reader?

I am implementing a low cost custom TouchGFX project using a stm342G071 and an ILI9488 based display. For the ILI9488 driver I need the touchGFX framebuffer in RGB888 format.This works ok if I keep the image data in internal flash but I need to put ...

TMack.1 by Associate II
  • 2192 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.