STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Static Graph logarithmic x-axis

I'm working on an GUI that has mainly a static graph wich plots bode diagrams. So i have been searching on the API of touch gfx ways to make a logspace in x-axis in order to plot frequency but a i didnt find a way to change the linear magnitude of x-...

0693W00000Uoi9MQAR.png
JPine.1 by Associate II
  • 5786 Views
  • 10 replies
  • 0 kudos

Backend Changing of framebuffer orientation

Hello. I saw a post about using a 180 orientation and did it, but as said, the performance was broken. Can i change the backend mounting of framebuffer? Where can i find where TouchGFX API is mounting framebuffer? There is another way, like changing ...

EKama.1 by Associate II
  • 1240 Views
  • 1 replies
  • 1 kudos

hardware integration

can i use stm32 hal libraray to interact touch gfx with hardware without using task and queue methods one of the video posted by st on youtubehttps://www.youtube.com/watch?v=qqCu3D3zhn4ie, functions and variables are used as extern simply write h an...

MA.21 by Associate III
  • 850 Views
  • 0 replies
  • 1 kudos

Resolved! Add Widgets, line, etc. at run time

Hello, is it possible to add for example a line on the canvas at run time? I'm managing to do a log x scale providing the decades separators with a Line object, but my plot could have more than one decade, so i think is a terrible idea to add many li...

JPine.1 by Associate II
  • 2112 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMx initialization bug

I found the following bug:STM32CubeMX generates the following initialization code: /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DCMI_Init(); MX_I2C1_Init(); MX_I2C2_Init(); MX_UART5_Init(); MX_USART1_UART_Init(); MX_D...

CJans.1 by Associate III
  • 2466 Views
  • 2 replies
  • 1 kudos

Resolved! DMA transfer error but CFSR does not indicate bus error

I'm using a STM32H743.I used STM32CubeMx to configure the DCMI. It uses DMA to transfer to memory.When calling HAL_DCMI_Start_DMA(), the DCMI_DMAError() function is called.I found out that there is a transfer error. And according the documentation a ...

CJans.1 by Associate III
  • 2540 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.