STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to use TouchGFX with STM32G0B1RE?

Hello!I would like to know if it is possible to develop a project in TouchGFX directed to the STM32G0B1RET6 microcontroller.According to the examples/documentation the STM32G0B1 is not supported.Please, could someone help me? Or do you have an exampl...

CVSta by Associate III
  • 2621 Views
  • 3 replies
  • 3 kudos

Resolved! How to use BW_RLE image format on a 16bpp LCD

I have a project that uses an arrow image in many parts of the UI. Currently the project has 5 different versions of the same image, but in different colours. I have limited flash space and would like to condense the 5 images down to 1 BW_RLE image. ...

KStea.1 by Associate II
  • 1572 Views
  • 1 replies
  • 1 kudos

Resolved! External Flash assets updates while touchgfx is running

Hi,I am implementing a product that uses touchgfx and needs to support remote updates. As the downloading of the assets is slow (~30min), the updated assets to be written into external flash must be written while touchgfx is running. I know that othe...

KHeye.1 by Associate III
  • 8376 Views
  • 13 replies
  • 1 kudos

TouchGFX Designer VS CubeMX pinout configuration for STM32H747I-DISCO FMC memory. Which is the correct one?

TouchGFX Designer version: 4.21.4CubeMX version: 6.8.1These are the pinout difference:Signal, Pin TouchGFX, Pin CubeMXFMC_SDCKE0, PC3, Not Mapped FMC_SDCKE1, Not Mapped ,PH7FMC_SDNE0, PC2, Not MappedFMC_SDNE1, Not Mapped ,PH6 FMC_SDNWE, PC0 ,PH5The D...

LChai.1 by Associate
  • 1604 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.