2023-05-29 11:23 AM
TouchGFX Designer version: 4.21.4
CubeMX version: 6.8.1
These are the pinout difference:
Signal, Pin TouchGFX, Pin CubeMX
FMC_SDCKE0, PC3, Not Mapped
FMC_SDCKE1, Not Mapped ,PH7
FMC_SDNE0, PC2, Not Mapped
FMC_SDNE1, Not Mapped ,PH6
FMC_SDNWE, PC0 ,PH5
The DevKit schematic corresponds to the CubeMX configuration. This makes me think that CubeMX generates the correct configruation for FMC SDRAM.
The project generated by TouchGFX designer works correctly launching from either TGFX Designer or STCubeIDE.
The questions are:
Thanks!!
2023-05-30 4:50 AM
Hello LChai.1,
There's no incorrect one. The TouchGFX board setup for STM32H747I-DISCO is preconfigured to be working with TouchGFX, and the pinouts are correct. But a project started from scratch with STM32CubeMX also has a correct pinout configuration, remember that there could be multiple pinout configurations that are ok.
So there's no bug in generated code, and of course, you can use TouchGFX Designer generated project.
/Osman
2023-05-30 6:25 AM
Hi Osman, thanks for your answer.
There's something I don't understand.
Let's consider the FMC_SDNWE signal, in the schematic is connected to PH5 port as CubeMX configuration. Touch GFX on the other hand configure PC0 as FMC_SDNWE signal, but PC0 in the schematic is used for some signal required for USB functionality.
So how can TouchGFX configuration be correct if the FMC_SDNWE signal is physically connected to a non-FMC related IC (USB instead)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.