STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to hide the "painter" for circleprogress widget

I want to hide the colored progress bar in circleprogress widget when there is no data. I can hide the whole widget but how can I keep the background image(a grey circle) in place. If i set the value to 0 there is still a small dot that remains. I as...

tarmogr by Associate III
  • 2216 Views
  • 3 replies
  • 0 kudos

Riverdi RVT101HVSNWC00 external flash programming fails

I have been trying to program the mentioned display. Whilst using TGFX 4.20.0 I can program an empty project then, generate code and upload from CubeIDE 1.9.0 without issue. Adding an image to the empty project and run target from TGFX works no probl...

markH by Associate III
  • 6371 Views
  • 9 replies
  • 0 kudos

touchgfx doesn't invalidate screen properly

hello everyone, I try to run TouchGFX on STM32F2 series MCU (Cortex-M3) by using Cortex-M0 core lib. The project built successfully and run TouchGFX. The screen seem good. But I have a problem, after the animations like slider, button pressed etc. th...

WhatsApp Image 2023-08-02 at 18.09.45.jpg
hsynk by Associate II
  • 2432 Views
  • 2 replies
  • 0 kudos

Using hardware buttons with SwipeContainer

I have to replace the touch screen gestures with hardware buttons іn "SwipeContainer" ;- sorry, but I couldn't find any native actions that can change the the pages in this container (in Designer4.22.0), so I tried to do it by my own.. Using "setSele...

DZhuk.3 by Associate
  • 2972 Views
  • 4 replies
  • 1 kudos

STM32H7: CM4 for TouchGFX, CM7 for the rest

Hello TouchGFX Community!It's not a question, but my findings.ST recommends to split tasks between two cores of STM32H7: CM7 for GUI, and CM4 for real-time tasks.In this configuration, we throw away all advantages of CM7 over CM4:- instruction cache-...

Ahper by Associate
  • 1500 Views
  • 0 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.