STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX animation documentation

I am using a custom STM32H743BIT6 board connected to a 480x272 display.  I have implemented several software products with this hardware and are working fine.  The issue I am having is I am trying to use the Animated Image for the first time.  After ...

RLarr.1 by Associate III
  • 1656 Views
  • 1 replies
  • 0 kudos

Heap Screen Storage Issue

Hi, I am currently trying to implement QRCode from qr-code-generator-library to display it on STM32F429I-DISC1 with TouchGFX. When I run it in the simulator on TouchGFX simulator it runs normally, but when I run it on the board it only shows whitescr...

Screenshot 2023-08-18 135216.png Screenshot 2023-08-18 135422.png Screenshot 2023-08-18 135509.png
Eshya by Associate
  • 1451 Views
  • 1 replies
  • 0 kudos

Resolved! TOUCHGFX While loop issue

Hello guys, I have a question. I am using touchgfx. When I use the while loop in my Model.Cpp file, the application stops. It does this without entering the while loop. Can't use loops in Model.Cpp? Do you have any knowledge about this topic?

amorftor by Associate II
  • 1813 Views
  • 1 replies
  • 0 kudos

scrollList HighLight scrolling item

hi all, I need to highlight an item in a scrolllist using two buttons that start scrolling up and down. I managed to implement the routine but I have problems as soon as the system passes into the area of the list that is not yet displayed. Does anyo...

TouchGFX double framebuffer not switching buffers

I am working on a gui using an STM32H747I-DISCO connected to an external 640x480 display. The external display does not have a DSI interface, so the DSI-related code in TouchGFX is commented out.The display works perfectly for static images, but heav...

nathan_s by Associate
  • 3162 Views
  • 1 replies
  • 0 kudos

Click on a widget without touchscreen

Hi,For a device without touchscreen, I'm prototyping a GUI using a clickable wheel as user input. A red box is used as visual focus on widget. I tied the following code to deliver a programmatic click :void navScreenView::selectClicked(){ Rect cli...

Fribes by Associate
  • 1596 Views
  • 1 replies
  • 0 kudos

How to reduce the memory flashing time when debug

Hi to all community.I am new with the touchgfx and the graphic ST microcontrollers.I have develop an application on STM32H7 MCU with touchgfx. The mcu use an external 16Mb flash memory to store the application, touchgfx, images etc...The graphic inte...

Ggual.2 by Associate II
  • 8620 Views
  • 12 replies
  • 5 kudos

Customized Nucleo board with changed MCU

Hello,I'd like to customize one of the current available demoboard (NUCLEO-G071RB) changing the MCU with a compatible one which I have purchased (STM32G0B0RET6).I've mounted this pin-to-pin compatible MCU (according to CUBEMX) on the aforementioned N...

Madrac by Associate II
  • 1936 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.