2023-09-01 3:35 AM
Hi,
I am beginner to TouchGFX , currently I am working on implementation of progress bar. requirement is I have to show progress bar based on user inputs. for example, if I have received 5 second as input, I need to show time increment and accordingly progress bar has to show progress. and at the end both timer and progress bar should complete the process at same instant.
Any suggestion about what best way is to implement this.?
Thanks in advance.
Regards,
jsalg.
2023-09-01 4:25 AM
Hello @jsalg.1 ,
There are multiple tutorials and an example in TouchGFX designer that shows how to use a progress indicator. You can read about them here:
https://support.touchgfx.com/docs/category/progress-indicators
I hope this would help you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.