STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

portability of the project to another computer

hello everyone, I have absolutely identical versions  TouchGFX 4.22.1 ; CubeIDE 1.13.1 ; CubeMX 6.9.1  on two computers win10.I’m creating a project in  TouchGFX  on the first computer, which takes up about 800MB, which I think is very strange, I don...

gevmar by Associate III
  • 2014 Views
  • 2 replies
  • 0 kudos

Resolved! External events as triggers

Hello dearIt would be very nice to give us a simple example to explain all your codes to order to change a widget on a screen.You tellus to use "TouchGFX HAL Development" in your example gpio https://support.touchgfx.com/docs/development/board-bri...

Roger3 by Associate
  • 8371 Views
  • 16 replies
  • 1 kudos

Resolved! play Video using STM32WB5MMG with Touchgfx?

hello everyone ,i have successfully using MX+TouchGFX+IDE with my custom PCB board,and i want to add a video into my project,but i can't find "LIBJPEG" in "Middleware and Software Packs" or "JPEG" in "Multimedia",like this website:https://support.tou...

yukang_0-1703044732711.png yukang_0-1703048569690.png
yukang by Associate II
  • 2480 Views
  • 3 replies
  • 0 kudos

Resolved! Disable touchGFX access to external flash temporarily

Hello all,I am developing a touchGFX application on STM32F7 with the frame buffer stored on an external QSPI flash. While app is running, I need to write data to this external memory but, to allow the flash write, I have to exit the memory-mapped mod...

CP??r by Associate II
  • 4491 Views
  • 6 replies
  • 2 kudos

Dynamic Graph background color

Hello, This seems like a basic question but I can't seem to find an answer anywhere: I'd like to change the background color of the dynamic graph from white to some other color (black ideally). This would be the entire background color I'm after, not...

RichH81 by Associate II
  • 2133 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.