STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Hour and minutes

Good morning , sorry if i'm not posting in the right place but i'm still learning. I have a problem with an example i saw in the tutorial where you bild an iterface to adjust the hour and minutes . In the tutorial where i built the interface it says ...

StefanoL by Associate III
  • 6650 Views
  • 16 replies
  • 6 kudos

Custom trigger

Hello, Is it possible to create a custom trigger for box shape?I would like to move the box using interaction, but I would like to trig this interaction from source code, is it possible? Thanks,Best regards,Laurent

lclor by Associate III
  • 2309 Views
  • 3 replies
  • 1 kudos

TouchGFX Run Simulator Fail

Hi,I tried to install TouchGFX 4.23.0 and 4.23.1 several times. OS is Win 11 pro eng/us region and eng language settings.When executed the run command on windows simulator fail message appears as in attachment.Also fails when creating any discovery b...

ali_ by Associate II
  • 12446 Views
  • 9 replies
  • 5 kudos

Upgrading TouchGFX engine and external buttons

This is an outstanding issue that's been there for a while but since it just got me again, I'm finally taking the time to post about it.  When using external buttons and the button controller, the implementation instructions have you edit the ToughGF...

Jazman by Associate III
  • 2341 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX Slider can be set in between values

The range of the default Slider of TouchGFX can be configured by a min and max integer.When the value has changed you can get a callback with the new value as an integer.Still when moving the slider it is possible to set the location of the indicator...

EmbDev by Senior
  • 3179 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.