STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX + ILI9341 16bit + FSMC

Hi,i have a simple question about the configuration in the subject:to drive the TFT can i use the "parallel RGB (FMC)"?If i must select the "Custom" interface can i use the X-CUBE-DISPLAY library for ILI9341?How this library must be interface with To...

Ivans91_0-1707779923390.png
Ivans91 by Associate
  • 3790 Views
  • 4 replies
  • 0 kudos

Resolved! Disable touch controller while running the code.

Hello everyone,I've been pondering the most effective method to disable touch functionality while running my application. It's crucial for me to do so because I'm developing an RF product that could potentially cause interference with touch inputs.Sh...

GMene.785 by Associate II
  • 1980 Views
  • 2 replies
  • 1 kudos

Resolved! TouchGFX safety/quality certification/compliance?

Hi,after looking into the library code, this forum, and playing for a while with library itself, I'm afraid I know the answer, - yet I'm still required to ask:does TouchGFX (or may be some current or future-planned variants of it) comply with any saf...

bear2023R by Associate III
  • 1458 Views
  • 1 replies
  • 0 kudos

Resolved! Touchgfx L8 Image Hard Fault Handler

Hello,I'm using a display with stm32f4 + external memory for image and font.The project runs well using flash in mapped mode.Now I want using flash in indirect mode because I need use part of it for storing info.I implement serial flash datareader an...

Ngard1_0-1709919971026.png
Ngard.1 by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.