2020-08-24 4:29 AM
and more, how the characteristic parameter this LCD has?
2020-08-24 6:43 AM
Hello,
What is this 7'' LCD ? Because it's not the one embedded on the F469-EVAL.
Please provide more information.
/Alexandre
2020-08-30 10:48 AM
In fact, I designed my work in touchgfx software on stm32f469 eval.
Now if I design a board exactly like the stm32f469 eval board and put a 7-inch lcd with a resolution of 480 x 800 on it, according to the touchgfx settings, will the code generated by touchgfx run on this hardware?
And my question is exactly what 7-inch LCD should I get so that I do not get into trouble?
Will the problem be solved just by changing the settings of the LTDC unit according to the 7-inch LCD?
2020-09-07 12:04 AM
Hello,
Yes in theory the code generated by CubeMX and TouchGFX should work.
For the screen, we don't have any recommendation in particular. If you choose a LTDC screen, this will simplify the implementation as LTDC is fully handled by TouchGFX Generator.
/Alexandre
2024-03-12 6:26 AM
I want to use a 7 inch and above screen with toucgfx and you do not know which screen I can use. So what use will this kit be if I can't make an original design and I can't even find the screen on it? I paid a ton of money for the stm32f469 i kit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.