STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGfx with ILI9341

Hi All,This is the first time I am posting on this forum. I am new to cubeIde/cubeMX world. I have recently started integrating the touchGFX capability to my stm32 boards. I followed some online tutorials and youtube videos like these:(https://www.yo...

TouchGFX Create a Count-down Timer

How do you create a graphical count-down timer in TouchGFX?Are there any example custom widgets that implement a count-down timer that I am not already aware of?It seems that the Model::tick() function's cycle time varies based on the LCD, so I am no...

Resolved! Touch gfx linkers

When i run target this message appeared plz help me '' Compiling Utilities/JPEG/jpeg_utils.cCompiling Common/Src/system_stm32h7xx_dualcore_boot_cm4_cm7.cCompiling ASM STM32CubeIDE/CM7/Application/User/Startup/startup_stm32h747xihx.sLinking CM7/TouchG...

Aziz by Associate II
  • 5409 Views
  • 10 replies
  • 1 kudos

STM32U535 + ILI9341 TouchGFX Performance

I'm using TouchGFX with a custom board that contains a STM32U535 and ILI9341 display.  The display also has the XPT2046 touch controller.  The issue I'm running into, which ControllerTech pointed out in his video, the touch/refresh is kind of spotty ...

Resolved! Touchgfx and HAL_GPIO_WritePin in simulator

This piece of code works if I transfer it to my board, but if I use the simulator in TouchGFX, I get an error: gui/src/model/Model.cpp:7:10: fatal error: main.h: No such file or directory #include "main.h". Screen1View.cpp#include "stm32f7xx_hal.h" /...

amigafan by Associate III
  • 3972 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.