STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Erreur Linking TouchGFX

I created a project with multiple screens and i want to recceive data and display them on the 4th screen so i created a task and a queue . I followed the MVP model and  int the model class i put the code in the tick function but when i run the code t...

Creating an TouchGFX Board Setup Fails

I'm trying to create a specific template for a custom board and following this stm link: https://support.touchgfx.com/docs/development/scenarios/scenarios-create-at I get the following error right on the first command.  C:\Users\user\Desktop>C:/Touch...

Board EVK070016 with MCU STM32H743XIH6

Hi all,as I'm stil new to STM and TouchGFX I'm facing the following problem.The GUI was developed using a EVK070016 Kit. This board uses a dispay resolution of 1024 px and a MCU STM32H750. For evaluation it works fine. Now I was told that real I(prod...

HaJott by Associate
  • 1711 Views
  • 2 replies
  • 0 kudos

How can I modify the framebuffer memory size?

In TouchGFX version 4.18.0, after modifying the Designer output for the screen and compiling with STM32CubeIDE, the screen crashes and restarts due to having too many screen elements (buttons, text, images). It’s suspected that this is caused by insu...

yu_jay by Associate II
  • 2118 Views
  • 2 replies
  • 1 kudos

Resolved! Slide controls implementation

Hi,if I understand correctly, TouchGFX does not support sliders. What is the simplest and safest way to implement them for a newbie to the ST ecosystem and tools?More specifically two types: scrollbars (of a text window) and date-picker wheel.As a si...

Ricko by Senior III
  • 1938 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.